Part Number: DS90UB953A-Q1
With the DMS CAMERA application
I'm trying to use DS90UB953.
I want to use IRLED+Camera as POC
Can you tell me the POC FILTER value of the maximum current value
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB953A-Q1
With the DMS CAMERA application
I'm trying to use DS90UB953.
I want to use IRLED+Camera as POC
Can you tell me the POC FILTER value of the maximum current value
Hello Young Jin,
In the DS90UB953 datasheet we provide an example PoC solution. The PoC solution provided corresponds to the part numbers shared in Table 8-1.
The example PoC solution is rated for a maximum current value of 150mA.
Best,
Zoe
To output a maximum current consumption of 400 mA
Please check if you can provide the POC FILTER value.
Hi Young Jin,
I am unable to share PoC solutions outside of the datasheet on this public forum. We have an additional PoC Application Note which is under NDA. Please reach out to your local TI sales office representative for the app note which will contain these solutions.
We also suggest working directly with vendors such as Murata, TDK, and Coilcraft for a custom solution if desired.
Best,
Zoe