Other Parts Discussed in Thread: ESD1LIN24
Hi Team,
Advantages of ESD1LIN24DYFRQ1 and general ESD electrostatic protection components,
Does LIN BUS have special specifications for ESD protection?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
Advantages of ESD1LIN24DYFRQ1 and general ESD electrostatic protection components,
Does LIN BUS have special specifications for ESD protection?
Hi Kevin,
ESD protection components will provide system level ESD protection according to IEC61000-4-2 and clamp ESD pulses to much lower voltages acceptable to sensitive circuitry.
Please see our app brief on LIN ESD Protection for further details.
LIN bus itself doesn't have special specifications for ESD protection to my understanding, that is at the discretion of the designer. There are many automotive projects that must meet test requirements according to a standard such as IEC62228-2 that will require ESD protection up to 25kV.
Regards,
Sebastian
Hi Kevin,
What general electrostatic protection components are you referring to here? Varistors? ESD diodes? Capacitors? Also what is the specific application here?
I would consider ESD1LIN24 a "general electrostatic protection component". It is an ESD diode that offers IEC ESD/Surge ratings and clamps overvoltage events above the breakdown voltage to protect sensitive downstream circuitry
Some of the specifications were tailored to accomodate LIN bus characteristics such as the working voltage of 24 V to protect the diode from short to battery events in 12 V battery automotive systems.
Regards,
Sebastian