This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1463-Q1: Quiescent current spec (VSUP current during Sleep mode)

Part Number: TCAN1463-Q1

Hello team,

I have a question regarding the quiescent current into VSUP pin during Sleep mode and how the specification in the datasheet can be interpreted.

In section 7.7 the current I_SUP_Sleep is specified with typ 18µA and max with 30µA. The test condition is in Sleep mode. But the general description mentions that V IO = 3.3V and Vcc = 5V, which would not be present in Sleep Mode. Is the spec also valid for VIO = 0V and VCC = 0V?

It is the same with picture 7-3, where several curves are shown for the current according to the input voltage of VSUP.

Are the values in the diagram typical values and how is a typical value defined (e.g. 3 Sigma)?

Thanks for your support and best regards,

Michael