Other Parts Discussed in Thread: TCA9548A
Dear TI Team:
Checked from PCA9548A datasheet, It shows it also supports voltage Translator function.
There are some items need your help.Thanks!
Pls check the picture as below, The PCA9548A is powered with 3.3V,
The main I2C is pulled up with 3.3V,
I2C7 is pulled up with 1.8V, I2C6 is pulled up with 3.3V,
1. This design is ok or not?
2. Main I2C switch to I2C6/I2C7 just with a transistor, how the PCA9548A guarantee the correct isolation between main I2C(3.3V) and I2C7(1.8V)?
3. Is there any relationship between the I2C0-I2C7 pull up voltage and PCA9548A power voltage?

Best Regards!
Lisa