Dear Specialists,
My customer encountered similar trouble.
Could you please let us know the way to PWRCTL1/BATEN1 high?
---
I powered on the TUSB4041 with the following configuration.
However, the output of PWRCTL1/BATEN1 did not become Hi.
Could you please tell me the conditions under which the output of PWRCTL1/BATEN1 becomes Hi?
USB_VBUS: PD(16kΩ)
OVERCUR*: 3.3VPU(4.7kΩ)
PWRCTL_POL: 3.3VPU(4.7kΩ)
AUTOENz/HZ_SUSPEND: 3.3V PU(4.7kΩ)
FULLPWRMGMT/SMBA1: PD(4.7kΩ)
GANGED/SMBA2/HS_UP: PD(4.7kΩ)
TEST: PD(4.7kΩ)
USB_R1: PD(9.53kΩ)
XI: 24MHz (3.3V)
---
I appreciate your great help in advance.
Best regards,
Shinichi