The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1043A-Q1: Regarding 1.8V VIO support in TCAN1043A-Q1 CAN FD Transceiver

Part Number: TCAN1043A-Q1

Hello team,

We need CAN FD transceiver with wake function which supports 1.8V VIO. I found TCAN1043A-Q1 datasheet which says it supports 1.8V VIO as per below screenshot but all the electrical parameters are given for condition VIO=3.3V (as per below screenshot) and also the lower limit of VIO is 1.7V. So I need confirmation that, whether this transceiver can be used for applications with 1.8V VIO completely.

Thank you in advance

Kavana H