This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB940-Q1: Help with 0x6c/6d indirect register setting

Part Number: DS90UB940-Q1

We are using UB940 pairing with UB947. While we can get normal image from one video source, another one has no display at all. We suspect that we need to change  0x6c/6d indirect register values in order to make it work. Here are the information we got for the input image. Please help us set the correct values for  0x6c/6d indirect registers.

horizontal front porch: 25 pixels

horizontal sync pulse: 3 pixels

horizontal back porch: 32 pixels

horizontal active: 800 pixels

horizontal total: 860 pixels

vertical front porch: 17 lines

vertical sync pulse: 4 lines

vertical back porch: 5 lines

vertical active: 487 lines

vertical total: 513 lines

frames per second: 60