This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCA4307: Low output voltage of PCA9544A compatibility with TCA4307

Part Number: TCA4307
Other Parts Discussed in Thread: PCA9544A, ADS1115

Dear experts,

I will connect the TCA4307 out I2C interface to the I2C of PCA9544A. The maximum low input voltage of TCA4307 is 0.4V but I can't find the low output voltage of PCA9544A in the datasheet. Only, in page 5 it is mentioned the low output current as 6-10 mA when Vol = 0.6V and 3-7 mA when Vol = 0.4V.

My question is: As I need to guarantee that low output voltage of PCA9544A to be <= 0.4V then please confirm that if I limit the low output current to 3 mA at VCC=3.3V then the low output voltage will never exceed 0.4V.

Regards,

Mohammad.