This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB638-Q1: Back Channel Frequency Select

Part Number: DS90UB638-Q1
Other Parts Discussed in Thread: DS90UB635-Q1,

I have a DS90UB638-Q1 / DS90UB635-Q1 system running.

I would like to test at a lower forward frequency.

Table 7-8 (Clocking Modes) of the 635 data sheet describes a Synchronous (Half-rate) mode.  I would like to test that mode.

I understand the first step is to configure the BC_FREQ_SELECT field in register 0x58 of the 638 device.

On power up, register 0x58 reads 0x1E, indicating a 50Mbps back channel was configured by the MODE Pin strapping.  This is expected.

I try to write 0x1D to change the mode to 25 Mbps back channel.

Register 0x58 always reads back 0x1E.

Am I missing some step in this configuration?