Part Number: AM26LS32A
Other Parts Discussed in Thread: LM339, TLV1814, ISO7740, AM26C32, AM26LV32E
Dear team,
The customer would like to use AM26LS32A for their Encoder application. Please review below customer question.
1. The absolute maximum rating of differential input voltage is +-25V at datasheet. How about recommended operating condition of differential input voltage?
2. The max operating voltage on 1A/1B port? Operating max voltage 1A or 1B is 7V?
3. It the customer use 0 to 12V on 1A, 12V to 0V on 1B port, is it operate well without damage?
Please let me know your opinion.
Thank you.