Part Number: DP83849IF
Other Parts Discussed in Thread: DP83869
Hello TI,
We are designing a device which needs ethernet connection so for interfacing with the host we need a phy IC having following requirements which they must bear:
- Datarate (Mbps) : 100/1000 (or only 1000)
- Interface Type : RGMII
- No. of ports : Dual (atleast)
I have mentioned a part number above ie; DP83849IF, it's all functions are sufficient for us but we need RGMII interface type and Datarate 1000 Mbps which is not present there.
So, please suggest some part numbers so that we can select any one of them which suits our product perfectly.
Waiting for your reply.
Thanks in advanced!
Regards,
Abhishek