Other Parts Discussed in Thread: DP83869
Tool/software:
Dear TI Support Team,
I hope this message finds you well. I am currently working on a project where I have interfaced the DP83869Hm Ethernet PHY with the MSP432P401R LaunchPad. The MDIO interface is connected to Pin P2.7, and the MDC interface is connected to Pin P2.6. Additionally, the GND connection is established as per the recommended setup.
Project Overview:
The objective of my project is to convert Ethernet copper (BASE-T) to Ethernet fiber. To achieve this, I need to configure the DP83869Hm Ethernet PHY appropriately.
Query Details:
- Accessing PHY Address:
- With the current hardware setup, how can I access the PHY address using the MDIO USB Tool?
- Configuration Requirements:
- Is it possible to perform the necessary configurations, such as setting the PHY address and adjusting other parameters, directly using the MDIO USB Tool without programming?
- Software Compatibility:
- Which software applications are compatible with the MDIO USB Tool for configuring the DP83869Hm Ethernet PHY?
- Additional Support:
- Are there any specific resources, documentation, or tutorials available that could assist me in effectively utilizing the MDIO USB Tool for configuring the DP83869Hm Ethernet PHY?
Project Details:
- Hardware Setup:
- MSP432P401R LaunchPad
- DP83869Hm Ethernet PHY
- MDIO interface connected to Pin P2.7
- MDC interface connected to Pin P2.6
- GND connection established
I would appreciate your prompt assistance as I am currently in the process of configuring the Ethernet PHY for my project.
Thank you for your attention to this matter. I look forward to your guidance and support in successfully configuring the DP83869Hm Ethernet PHY for my project.