Other Parts Discussed in Thread: TUSB8041,
Tool/software:
Hi Team,
customer want to know the 8 inches between host to HUB or HUB to device. Would you please help me to answer this question?
![]()
Many thanks~
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,Yadong
Section 11.1.3 describes the layout recommendations for all the TUSB8041 differential pairs: USB_DP_XX, USB_DM_XX, USB_SSTXP_XX, USB_SSTXM_XX, USB_SSRXP_XX, and USB_SSRXM_XX. So the 8in requirement applies toward both the TUSB8044A upstream and the downstream ports using FR4 and standard 6 layer stackup, The insertion loss will vary based on board material and stack up. We can also review their layout to help them achieving the best signal integrity.
Thanks
David
Hi Daivd,
If host to HUB up to 6 inches and HUB to device up to 6 inches, and used the cable will cause -2db lose. Does the TUSB8044A support it?
many thanks~
Hello,
Due to a US Holiday, the response to your question may be delayed. We will look into your question when we return tomorrow, July 5th. Sorry for the wait and any inconvenience it may cause.
Thanks,
Ryan
Yadong
Is this a standard USB cable? Where is the cable being used?
The 8in guideline given in the datasheet assumes the host and the hub are on the same PCB without the external cable.
Thanks
David
Hi Yadong:
There is hub layout guidance in datasheet on page 57.
Regards
Brian