Part Number: SN65HVD1050
Tool/software:
Dear Team's,
We have used SN65HVD1050DR for can bus communication in our designs. I check the CANL waveform found that CANL voltage is 2.5V is over specification 1.5V.
Is CANL voltage above 1.5V an issue?
How can I modify the circuit so that the CANL voltage is lower than 1.5V?
Circuit: CN301 is not connected to anything.

Waveform: CH1-CANL, CH2-CAHH, CH3-VREF

SPEC: