This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65HVD1050: SN65HVD1050DR CANL voltage level over specification

Part Number: SN65HVD1050

Tool/software:

Dear Team's,

We have used SN65HVD1050DR for can bus communication in our designs. I check the CANL waveform found that CANL voltage is 2.5V is over specification 1.5V.

Is CANL voltage above 1.5V an issue?

How can I modify the circuit so that the CANL voltage is lower than 1.5V?

Circuit: CN301 is not connected to anything.

Waveform: CH1-CANL, CH2-CAHH, CH3-VREF

SPEC: