Part Number: DS100DF410
Other Parts Discussed in Thread: SIGCONARCHITECT
Tool/software:
We are working on waveform improvement for burst and continuous signal using DS100DF410.
We use SigCon Architect for configuration changes.
Question 1: When the signal is continuous and the CDR is unlocked and the Retimed data is set, what kind of processed signal is being transmitted?
We believed that if the CDR is not locked, there would be no Retimed data signal at all. But in fact, a waveform was detected.
Question 2: In the CDR unlocked state and burst signal, we want to achieve the best signal waveform.
If there are any optimal settings that do not involve the CDR when it is unlocked, other than Rx EQ/DFE and Tx DEM/PRBS Generator?