This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPD6E001: transient suppressor

Part Number: TPD6E001
Other Parts Discussed in Thread: SN75240, SN65220, SN65240,

Tool/software:

I would like to know the opinion of your support for the choice of the most suitable transient suppressor for the MAX3344 transceiver. Since my USB device, which uses the MAX3344, and complies with the USB 2.0 standard and is Full-Speed, a high-capacitance (35 pF) suppressor such as the SN65220, SN65240 and SN75240 should be assigned to it. However, I am also using the FTDI FT4232HL, which also complies with the USB 2.0 standard, but is a High-Speed device. For this device a lower capacitance (1.5 pF) suppressor is needed, such as the TPD6E001RSER. Therefore I would like to know: Would it be feasible to use the TPD6E001RSER for both devices or would this mean that the Full-Speed device would lose too much protection?