This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS25CP114: Please tell me about the failure mode of DS25CP114TSQE.

Part Number: DS25CP114


Tool/software:

Hello teams.

Please tell me about below questions.


Q1. If a signal exceeding the IO rating is applied to either IN1 or IN2, is there a possibility that both S30 and S31 will short to GND?
(The board is designed with S30 = 3.3V: high, S31 = GND: low)

Q2. If an overvoltage is applied to S30 (fixed high), is it possible that S31 will also short to GND?
(The board is designed with S30 = 3.3V: high, S31 = GND: low)

Best regards,
Akashi