Tool/software:
I’m using a SN55LVCP22A-SP as a splitter. What do I do with the unused differential input? I’d assume I float it but what’s the recommended connection?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
I’m using a SN55LVCP22A-SP as a splitter. What do I do with the unused differential input? I’d assume I float it but what’s the recommended connection?
The inputs must not be left floating, and the two pins should not have the same voltage (but the input has some hysteresis, so it might work). Input voltages above 3 V are not recommended.
Hello,
I would recommend reading section 9.2.3.1 Design Requirements for reference.
Thank you,
Amy