This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83867IR: Ethercat 100Mbit compatibility

Part Number: DP83867IR
Other Parts Discussed in Thread: DP83630

Tool/software:

Dear,

is DP83867IR connected using MII interface compatible with Ethercat 100M (100Mbits, standard ethercat)?

The MII interface is controlled by the Beckhoff ESC of the MCU.

In Beckhoff application note I can see that DP83867IR is listed, but only for the Ethercat 1G section (all the PHY listed in the 100M section are 100M only PHYs).

In alternative is it possible to receive a P/N suggestion for an Ethernet PHY compatible with Ethercat (MII connection required) that is also able to support TSN?

For TSN compatibility I am talking about 802.1AS/AS-rev, 802.1Qbv and 802.1CB.

I serched a little bit in Texas Instruments website but the only PHYs that provide TSN support are 10/100/1000 PHYs, there is no non-Gigabit ethernet PHY that supports TSN.


TSN (Standard Ethernet 100Mbit) and Ethercat are not meant to work at the same time on the same application, but in different usecases, but the desire is to use the same Ethernet PHY for both.

Let me know if you need further information

Best regards

Alessandro