This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPD4E05U06-Q1: Can this part provide protection for short to 48V VBUS?

Part Number: TPD4E05U06-Q1
Other Parts Discussed in Thread: TPD4E05U06

Tool/software:

Hello experts,

I am using this device for the USB Type-C SuperSpeed signals, which are right next to VBUS pins, and USB PD can be as high as 48V.

I also have AC coupling caps on the SuperSpeed lines.

With the AC coupling caps, is the TPD4E05U06-Q1 capable of protection against short to 48V VBUS?

Thank you and best regards,

Seong