Part Number: MAX3221
Other Parts Discussed in Thread: OPA211, OPA132,
Tool/software:
Hello everyone,
I have an interesting project where I need to create a line driver that can signal across thousands of feet of cable. Cable will be between 75 and 110 ohm and between 1.2 and 1.7 uF.
Our target is between 40 and 200 kbaud.
For reference we are currently do 50kbaud by feeding our CMOS level outputs into a OPA211 that then buffers to a push pull BJT to signal 30 VP2P. Simple but effective:
I am wondering if switching to OPA132 or possibly MAX3221 (we are open to sending RS232) would yield better results or should we take steps to improve the circuit design from another IC.
Min and max baud rates will be 50k and 200k so I am calculating a minimum slew of 4.7V/us and to reach full speed 18.8V/us.
Also, to lower ISI we only pulse on transition instead of entire clock cycle. For example:
I'd like to be able apply pre-emphasis to the pulses but don't see any solutions that build that into an IC beyond the MAX3221.
If anyone has experience with extreme cable length signaling, open to try new ideas.