This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TSWDC155EVM: Unable to connect to the TSWDC155EVM via JTAG

Part Number: TSWDC155EVM
Other Parts Discussed in Thread: ADS9817EVM, , ADS9817

Tool/software:

Hi team,

Our customer is using TSWDC155EVM to evaluate ADS9817EVM for system performance.

The EVMs work well with the GUI, but when customer use JTAG or USB-C to directly connect to the TSWDC155EVM, the PC can not recognize the FPGA card.

The customer uses Xilinx Vivado 2020.1 for FPGA programming.

The boards are powered up correctly according to the GUI manual.

Could you help to confirm:

  1. Is the TSWDC155EVM accessible via JTAG / USB cable, and programmable externally? Or it can only be accessed / programmed by the EVM GUI?
  2. Can we provide source code or other programming support for this EVM?

Thanks,

Frank