This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB321: Validating concept of Host charging using Configuration Channel Logic and Port Control with VCON

Part Number: TUSB321
Other Parts Discussed in Thread: TUSB320, TUSB320-LA-EVM

Tool/software:

Hello Support Team,

My name is Mihir. I am working as an Embedded Engineer at Aimtron Technologies.

Meanwhile, our team is working on developing a product for audio domain which has the facility of USB Hub for connecting more than one USB Device with the product and transmitting/receiving data simultaneously without any interruption. Along with that, the customer emerges the with new requirement in which, the up-stream port of USB Hub must charge the Host device (i.e., MacBook, iPad, Mobile) that is communicating with the up-stream port of product.

As we are new in this feature, we require to validate the concept and identified that is it feasible or not. We have done some research about it but still we have not able to identify any scheme which we can implement to accomplish the design.

Can we charge the device which is connected on up stream port of Hub using TUSB321 without PD IC/ Controller?

Therefore, we would like to ask that do you have any reference IC or scheme which can be implemented in our design. If you have, then let us inform so we can move towards the validation and development.

Regards,

Mihir