This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83869EVM: Help with Fiber-Electrical Conversion

Part Number: DP83869EVM
Other Parts Discussed in Thread: DP83869, USB-2-MDIO

Tool/software:

I have SFP1G-SX-85, that converts fiber to electrical and vice-versa. That is inserted/used in the DP83869EVM board; and I am using an Ethernet cable connected to the AM62b-p1 starter kit evm board (set it to static IP).

I have Windows connected via Ethernet to UMC-GA1F1T, which also has SFP1G in it. So the hardware connection looks something like this -  PC>UMC-GA1F1T>DP83869EVM>AM62b-P1 board.

When I try to ping, it doesn't work, but when I replace DP83869EVM with UMC-GA1F1T, it works.

So my question is, do I need to do any hardware changes/configurations, like changing those DP switches or something, in order for it to work as mentioned above? (Totally newbie on this board.)

Currently on board I see LD2, LD4 an  d on and LDr is blinking. D1 is on with red-yellow in it, and all other 4 leds are on: 5V_Supply, FX3v3, VDDA2P5, and VDDIO.