Part Number: AM26LV31
Other Parts Discussed in Thread: AM26LV32,
Tool/software:
Hello,
Greetings !!!
Can you provide some reference circuit for AM26LV31 (driver) and AM26LV32 (receiver)?
There are some reference that I have taken from internet, where I could see 120ohm resistance is added in between input(+) and input(-) of receiver, and also pull up of 2K ohm is connected between input(+) and Vcc and pull down of 2K ohm is connected between input(-) and Gnd. Is it mandatory? if yes, what should be done with the driver input line?
Thanks in advance,
Saravanan