Part Number: ESDS452-Q1
Other Parts Discussed in Thread: ESDS552, ADS1261, ESDS452
Tool/software:
This TVS diode array is drawn as two separate bidirectional TVS diodes in the datasheet:

The working voltage is +-5.5v, so I'd expect IO channel 1 to be able to handle +-5.5v, and channel 2 to handle +-5.5v.
But if I put +5v on the first channel, and -5v on the second channel, it conducts as if it was internally constructed like this:

Which is absolutely not what the diagram in the datasheet implies, and also isn't how other dual channel TVS I have used before have behaved like.
For example, this dual bidirectional TVS from Diodes Incorporated does not have this unwanted behavior:
https://www.diodes.com/assets/Datasheets/DESD3V3L2BTQ-DESD24VL2BTQ.pdf
- Is there a part of the datasheet that implies this limitation?
- Is there an alternative part I can use?