Part Number: TCAN1044V
Other Parts Discussed in Thread: TCAN1044A-Q1
Tool/software:
Hello TI Team,
I am using the TCAN1044AVDRQ1 and would like to know the supply current on VCC behavior under following conditions:
- VCC = 5V, VIO=3.3V
- STB is changed from 0V to 3.3V.
- VIO is cut and left floating (effectively 0V).
I have noticed that if MCU is shut, it will source from the CANRX/CANTX pins (approx. 20mA), and I want to avoid this. So, during standby, if VIO is left floating, will the CAN IC be standby mode?
Regards,
Abhishekh