Other Parts Discussed in Thread: XIO2001EVM, PCI1520
Tool/software:
Hi Brian
I apologize for the late reply on my part. We were forced to focus on other parts of the project and then summer vacation also took some time.
We are now ready to proceed with this issue.
As requested in the other post (which is now locked), "yes, I need register info for PCMCIA card to compare." here are the register read out from the commercial PCMCIA board connected to the XIO2001EVM setup:
-> pciConfigSpaceShow 2,1,0
00: ac55104c 02100007 06070001 00824010
10: b0801000 020000a0 40030302 b0880000
20: b08bf000 b0840000 b084f000 0000f000
30: 0000f7fc 00000000 00000000 01400130
40: 12345678 000003e1 00000000 00000000
50: 00000000 00000000 00000000 00000000
60: 00000000 00000000 00000000 00000000
70: 00000000 00000000 00000000 00000000
80: 2844f060 00000000 00000000 00c01d02
90: 606000c0 00000000 00000000 00000000
a0: 7e020001 00c00000 0000081f 0000000b
b0: 08000000 00000000 00000000 00000000
c0: 00000000 00000000 00000000 00000000
d0: 00000000 00000000 00000000 00000000
e0: 00000000 00000000 00000000 00000000
f0: 00000000 00000000 00000000 00000000
value = 40 = 0x28 = '('
-> pciConfigSpaceShow 2,1,1
00: ac55104c 02100007 06070001 00824010
10: b0800000 020000a0 40040402 b08c0000
20: b08ff000 b0850000 b085f000 0000f800
30: 0000fffc 00000000 00000000 01400130
40: 12345678 000003e1 00000000 00000000
50: 00000000 00000000 00000000 00000000
60: 00000000 00000000 00000000 00000000
70: 00000000 00000000 00000000 00000000
80: 2844f060 00000000 00000000 00c01d02
90: 606000c0 00000000 00000000 00000000
a0: 7e020001 00c00000 0000081f 0000000b
b0: 08000000 00000000 00000000 00000000
c0: 00000000 00000000 00000000 00000000
d0: 00000000 00000000 00000000 00000000
e0: 00000000 00000000 00000000 00000000
f0: 00000000 00000000 00000000 00000000
value = 40 = 0x28 = '('
->
The readout is performed with the same SW on our PC, running the VxWorks OS.
Please advise if this clears anything up or if you need anything further from our side.
Regards
Lars