Tool/software:
Hi Team,
My customer encounter some question about TUSB4041I application, may I have your support on below items? Thanks!
1. According to the specifications described below, when the upstream port is connected, only CDP is supported, while when not connected, DCP can be supported. Is this difference influenced by the VBUS detection status of the upstream port? If not, what influences it?

2. In automode mode, Port 1 does not support CDP. Which mode does it support?

3.
1) If we want to use the automode function, does the upstream port not need to be connected? (In our actual application, the upstream port is connected long-term)
2) If the hub is to be used as a self-powered standalone USB hub product, how should the VBUS of the upstream port be connected?

4. What does the Bat Charging support function of the downstream port mean? Does it only indicate whether there is power in the VBUS of the downstream port?
5.
1) If J2 is to use the TYPE-C port and DN1_VBUS is to remain normally off (powering on only when a device is detected), how should pin4 PWRCL1/BANTEN1 behave?
2) If we want to use an MCU to control the power on/off state of DN1_VBUS, how should PIN4 and PIN14 behave?