Part Number: TLIN1431-Q1
Hi,
In pg no:43, I could find the reference calculation for calculating safe trigger area of watchdog service.
I have performed the same calculation and I like to know if it is correct i.e it considers all worst case scenarios and I haven't left anything.
In pin mode control, we are connecting it to GND and hence the total window size configured (Closed+open) is 32ms to 48ms.
1)In pg no: 43, 10% oscillator tolerance is considered. Whether 32ms to 48ms already considers this tolerance (or) do we need to add separately i.e 32ms becomes 28.8ms and 48ms becomes 52.8ms so that total window size becomes 28.8ms to 52.8ms?
2)Based on the consideration that 10% tolerance is already captured in 32ms to 48ms, I have estimated that worst case safe trigger area as 8ms & we have to service our watchdog every 28ms ± 4ms. Is that correct? (attached image for your reference)

Thanks,
Sri Viswa