Part Number: SN65LVDS93B-Q1
Hi Team,
I am planning to use the SN65LVDS93B-Q1 to convert the RGB signals from my host processor to LVDS for my display. My host processor has native RGB565 display signals (16-bit). My initial thought was to use the display example in Figure 14 on page 19 of the SN65LVDS93B-Q1 datasheet, which shows an 18-bit configuration, and then just ground the inputs for the two bits (Red and Blue) that are not used in the RGB565 configuration.
I was originally thinking that I should ground the two LSBs on the SN65LVDS93B-Q1: D0 for Red and D15 for Blue. Then I realized that the difference between the 24-bit example and the 18-bit example has the MSBs grounded and not the LSBs, so I thought I should ask here first to clarify.
For using the SN65LVDS93B-Q1 in RGB565 (16-bit) configuration, should I ground D0 for Red (treating D6 as MSB and D1 as LSB), or ground D6 (treating D4 as MSB and D0 as LSB)?
Likewise for Blue, should I ground D15 (treating D22 as MSB and D18 as LSB), or ground D22 (treating D21 as MSB and D15 as LSB)?
Regards,
Marvin