Other Parts Discussed in Thread: PCA9554, PCA9555, PCA9554A, TCA9535
Dear Sir:
May I have some question regarding TCA9555?
Regarding the TCA9555PWR, can pins P00 through P17 be configured only as Input (I) or Output (Open Drain) only, or can they also be configured as Input(I) or Output (O) and Output (Open Drain)?
Double confirming below mention Is that correct? :
If config Output (O) because TCA9555PWR pins P00 through P17 is push pull,therefore no need external pull resistor.
If config Output (Open Drain) TCA9555PWR pins P00 through P17will need external pull resistor.
Thanks