Part Number: TCAN1043N-Q1
Other Parts Discussed in Thread: TCAN1043, TCAN1043-Q1, , TCAN1043A-Q1
Hello,
We are evaluating the following components for a new Automotive ECU, ASIL C, 24 V system, with a load dump requirement of 58 V:
-
TCAN1043A/N‑Q1
-
TCAN1043‑Q1
-
TCAN1043H‑Q1
We have observed the following:
-
The TCAN1043N‑Q1 has a VSUP and load dump maximum rating of 45 V, which does not align with the CANH/L fault tolerance of ±58 V.
-
The TCAN1043‑Q1 has a VSUP rating of 58 V, but the datasheet does not explicitly specify load dump capability. We have also seen recommendations to transition to the newer TCAN1043A/N‑Q1.
-
The TCAN1043H‑Q1 appears to be the only variant that meets our requirements.
Could you please confirm:
-
Is the TCAN1043H‑Q1 indeed the appropriate choice for a 24 V system with a 58 V load dump?
-
Is it correct that the TCAN1043A/N‑Q1 cannot withstand a 58 V load dump?
Thank you very much for your support.
Best regards,