Part Number: ESD2CANFD24-Q1
Other Parts Discussed in Thread: STRIKE, ESD2CAN24-Q1
Hello team ,
I am trying to replace the part from nexperia PESD2CANFD with ESD2CANFD , all the features Vcl ,Vbr Vrw ,Ir and dimensions looks perfect ,only concern I have is Power dissipation .in the datasheet it is mentioned 133W but for the exixsting nexperia part it is 200W.
My question is
1.during the ESD pulse strike 8/20us from the generator in the CAN line 8kV or 15kV ,do we need to bother about power dissipation ? since the part already been qualified for CAN line and it is complaint with the standard
2.If yes to the above question , how do we calaculate and average the PD for ESD diode for 8/20us pulse
3.Please give me the calculation I have to consider ( ex- Ipp ) for 330ohm , 330pF generator specifications for calculation