Part Number: TS3USB221
Hi
The TS3USB221RSER schematic is shown in the diagram below. It is used to switch between USB 2.0 D+/D- and UART debug TX/RX outputs to the USB Type-A connector.
The UART (UART1_TX_3V/UART1_RX_3V) is connected to the CPU i.MX6 via a 3.3V/1.8V level shift IC. The USB 2.0 (USB_HUB_DP2/USB_HUB_DM2) is connected to the USB HUB as shown in the diagram below.
The HUB's power source is connected to the CPU i.MX6.
Phenomenon Description:
1. When powered off, if a USB flash drive is plugged into the Type-A connector and the device is powered on, the TS3USB221RSER has a certain probability (20%~50%) of causing the USB HUB to fail.
2. The same test with a keyboard/mouse plugged in fails.
3. Removing R434 (UART1_TX_3V defaults to 3.3V, suspected to be a source of interference) and 1D+... After grounding, the circuit tested normal 1800 times.
What are the possible causes and suggested solutions?