Part Number: SN65LVDT125A
Other Parts Discussed in Thread: SN65LVDS125A
Hello Team,
We are planning to use the IC SN65LVDT125A in one of our products.
The use case seems little differnt from the intended application of the IC.
We have an MCU which acts as an SPI master. The SPI slave is another device and is conneted via cable.
So we are converting this single ended SPI to LVDS with LVDS driver SN65LVDS31PW and LVDS receiver SN65LVDS32PWR (for MISO signal).
At the slave side, these signals are converted to single ended from SPI with transcivers MAX9111EKA+T and MAX9110EKA+T.
The SN65LVDT125A will be used at the slave side to switch the slave with different masters in the test bench.
The output side (Y&Z) will be connecteed to the slave and inputs (A&B) will be connected to differnt maters via connectors and vice versa for the MISO signal.
1). Can you please confirm the logic compitability of SN65LVDT125A with SN65LVDS31PW, SN65LVDS32PWR, MAX9111EKA+T and MAX9110EKA+T. ?.
2). if the driver is not seleceted with (xDE pin) or the forst output channel (1Y&IZ) are seleceted for the input 1A&1B thosugh the ouput channel selcection pins, what will be the signal at the non selected output channels due to paracitic capacitance between input and output?.
3).
Looking for your reply.