This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6748: Regarding the drive capability issue of the EMIFA interface of TMS320C6748

Part Number: TMS320C6748

 

When designing an application using the TMS320C6748, we utilized its EMIFA interface and connected 6-8 external modules. Due to structural design considerations, the routing length of the EMIFA interface is quite lengthy, reaching nearly 15000mil. Additionally, there is inter-board communication involved. I would like to inquire whether it is necessary to add a buffer on the signal line of the EMIFA interface to enhance its driving capability. Thank you.