Hello,
For our new project, I are evaluating the DS90UB903Q-Q1/4Q SER/DES. I have already bought the Evaluation Kit. Both Ser/Des working very well.
But a few days ago, when I search on web some alternative, I found DS92LX2121/22 SER/DES. I read very well the two datasheets and the main differences that I found, are the max values of input PCLK support (43MHz vs 50Mhz) and data throughput(903 Mbps vs 1050 Mbps). It is correct? There aren't any other functional differences?
Please you can confirm that Built in Self Test (BIST) is only available in the Camera mode? There is none way to implement this test or a BER test in Display Mode?
Thank you very much
Luca Tosetti
Imaging Division - R&D Department
Cefla Sc - Dental Group