Hi all.
There is a question about "SN55LBC173."
Is "-5V" output possible in the following pin states?
About 1.5V is inputted into B-input.
3.3V or 0V is inputted into A input.
VCC is connected to 0V and GND is connected to -5V.
Is the same usage possible also about "SN55LBC175"?
and, Is the same usage possible also about "DS26LV32-MD8"?
Best Regards.
Hisa Kobayashi.