Other Parts Discussed in Thread: DS90CF388A
Hi,
Is it required to have the same number of input channels on a receiver as there is there is being transmitted for LVDS? For example, if I were using the DS90CF388A (which can receive up to 8 channels) but I had something like the FCB-EH3150 from Sony (which is transmitting only 5 LVDS channels), are they compatible? I see no reason why all of the reciever channels would have to be used.
If not, are there any options from TI that I am missing that would have 5 LVDS receiver channels?
Thanks!