I have an application that requires up to 1200V between the input side of an isolator and the output side. I see from the specifications in the ISO721 datasheet that it lists a working "insulation" of 560V-peak. Does this mean that I should not use this isolator? Are there other isolators that are at least 100Mbps that could meet my 1200V requirement?
Thank you