Other Parts Discussed in Thread: SN65LVEP11
Dear TI-er.
What is the maximum junction temperature value of SN65LVEP11 ?
Plz help me.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: SN65LVEP11
Dear TI-er.
What is the maximum junction temperature value of SN65LVEP11 ?
Plz help me.
Hi Kiyoung,
Nice to see you.
Actually there's no data about the max junction temperature. But we can calculate from the following formula.
And all the parameter can be got from the datasheet. We can see the table from page 2 of the datasheet.
Let's take SOIC, Low-K as an example.
If temperature is less than 25C, then Tj=25+(139*0.719)=124.9C
If temperature is 85C, then Tj=85+(139*0.288)=125.03C
So we can know the Max Junction temperature is 125C.
If we take other package or High-K as an example, the result, 125C would be calculated, too.
So the answer you wanted is ,,,,,125C
Thank you for choosing our products!
Best regards!