This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Difference between SN65LVPE502 and SN65LVPE502CP

Other Parts Discussed in Thread: SN65LVPE502CP, SN65LVPE502, SN65LVPE502A, SN65LVPE512

Dear Specialists

My customer is thinking SN65LVPE502CP.

He wants to know the difference between SN65LVPE502 and SN65LVPE502CP.

According to the datasheets, the differences may be TRANSITION AMPLITUDE and OUTPUT DE CONTROL.

Could you please see attached file.

Does it have any other difference?

He has some use cases and wants to use the most suitable device for USB3.0 connection.

Best regards,

Shinichi

difference between SN65LVPE502 and SN65LVPE502CP.xlsx 

  • Hello,

    The SN65LVPE502CP is an old design and we rather recommend to use the SN65LVPE512 or the SN65LVPE502A, since both have fixes to known bugs on the SN65LVPE502CP, like the errata www.ti.com/.../sllz070

    Best regards,
    Diego.
  • Dear Diego

    Thank you for your reply and advise.

    I'll feedback the information of SN65LVPE512 to the customer.

    In this case, the customer is evaluating SN65LVPE502A, but it has a problem that compliance test isn't executed.

    When the device is removed, there are no repeater,compliance test is executed. there is no problem.

    So customer is considering to confirm from SN65LVPE502A to SN65LVPE502 or SN65LVPE502CP.

     It is required the differences between the devices.

    Could you please confirm attached file.

    Also advise following questions.

    (1)What is the reason SN65LVPE502CP devolopped?

    (2)Why has CM function deleted from SN65LVPE502CP? 

    Best regards,

    Shinichi

    difference between SN65LVPE502, SN65LVPE502CP and SN65LVPE512.xlsx