Hello team,
I'm trying to determine if the SN65LVDS391 can be used as a driver for a mini-LVDS reciever. The specs for the mini-LVDS receiver are as follows:
Parameter |
Symbol |
Min. |
Typ. |
Max. |
Unit |
Conditions |
Mini-LVDS High Input Voltage |
VIH |
75 |
100 |
_ |
mV |
|
Mini-LVDS Low Input Voltage |
VIL |
_ |
-100 |
-75 |
mV |
|
Mini-LDS Common Input Voltage Range |
VCM |
.4 |
_ |
Vcc-1.2 |
V |
|
Mini-LVDS Input Differential Voltage |
VID |
150 |
200 |
2000 |
mV |
Setup and hold time = 300ps Vcc = 3.0-3.6 |
Mini-LVDS Input Leakage Current |
IDL |
-1 |
_ |
1 |
uA |
|
The differential specs for our SN65LVDS391 are:
I'm trying to make sense out of these specs to make a confident decision:
The mini-LVDS receiver can detect a differential signal as low as 150mV (min. VID). Is it correct to say, for a worst case scenario, our SN65LVDS391's differential logic swing is min 247mV +/- 50mV, so it can be as low as 197mV, which is still enough for the mini-LVDS to detect the differential swing? Will the SN65LVDS391 be a good driver for this mini-LVDS receiver?
If not, what is our best offering for this application. Thanks.