Hello Team,
To use TPS65982EVM as load simulator in UFP configuration (while using TPS25810 as DFP), below are some quires.
1. We connected the Type C cable from DFP board (TPS25810EVM) to this board (J1), still we need to give power to J4 connector?
2. If we are not providing power on J4 connector then do we need to provide the external 3.3V power to J5 Connector?
3. Where to connect the DC load from this board?
4. Do we have any GUI to set the configurations?
Pl guide us for the connection to use this board in UFP configuration.
Regards,
Mahendra Patel