Hello, We are embarrassed.
Which standard is SN65LBC031? ISO11898-2 or ISO11898-3?
Also, is this device SAE CLASS B?
Thanks & Regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello, We are embarrassed.
Which standard is SN65LBC031? ISO11898-2 or ISO11898-3?
Also, is this device SAE CLASS B?
Thanks & Regards,
Both standards, and Yes it can be used for SAE Class B (see bottom of page). regards, Thomas
ISO 11898-1:2003 specifies the data link layer (DLL) and physical signalling of the controller area network (CAN). This document describes the general architecture of CAN in terms of hierarchical layers according to the ISO reference model for open systems interconnection (OSI) established in ISO/IEC 7498-1 and provides the characteristics for setting up an interchange of digital information between modules implementing the CAN DLL with detailed specification of the logical link control (LLC) sublayer and medium access control (MAC) sublayer.
ISO 11898-2:2003 specifies the high-speed (transmission rates of up to 1 Mbit/s) medium access unit (MAU), and some medium dependent interface (MDI) features (according to ISO 8802-3), which comprise the physical layer of the controller area network.
ISO 11898-3:2006 specifies characteristics of setting up an interchange of digital information between electronic control units of road vehicles equipped with the CAN at transmission rates above 40 kBit/s up to 125 kBit/s.
ISO 11898-4:2004 specifies time-triggered communication in the CAN. It is applicable to setting up a time-triggered interchange of digital information between electronic control units (ECU) of road vehicles equipped with CAN, and specifies the frame synchronisation entity that coordinates the operation of both logical link and media access controls in accordance with ISO 11898-1, to provide the time-triggered communication schedule.
ISO 11898-5:2007 specifies the CAN physical layer for transmission rates up to 1 Mbit/s for use within road vehicles. It describes the medium access unit functions as well as some medium dependent interface features according to ISO 8802-2. This represents an extension of ISO 11898-2, dealing with new functionality for systems requiring low-power consumption features while there is no active bus communication.
|
Product Code: J1850
Date Published: 2006-06-07Date Reaffirmed: June 2006
Issuing Committee:Vehicle Architecture For Data Communications Standards
ScopeThis SAE Standard establishes the requirements for a Class B Data Communication Network Interface applicable to all On- and Off-Road Land-Based Vehicles. It defines a minimum set of data communication requirements such that the resulting network is cost effective for simple applications and flexible enough to use in complex applications. Taken in total, the requirements contained in this document specify a data communications network that satisfies the needs of automotive manufacturers. This specification describes two specific implementations of the network, based on media/Physical Layer differences. One Physical Layer is optimized for a data rate of 10.4 Kbps while the other Physical Layer is optimized for a data rate of 41.6 Kbps (see Appendix A for a checklist of application-specific features). The Physical Layer parameters are specified as they would be detected on the network media, not within any particular module or integrated circuit implementation. Although devices may be constructed that can be configured to operate in either of the two primary implementations defined herein, it is expected that most manufacturers will focus specifically on either the 10.4 Kbps implementation or the 41.6 Kbps implementation depending on their specific application and corporate philosophy toward network usage. However, low-volume users of network-interface devices are expected to find it more effective to use a generic interface capable of handling either of the primary implementations specified in this document.
|
Thomas-san,
Thanks for your answer with faster and kindly explanation.
Thank you very much!