Part Number: TMDS141
Hi,
Our customer has a question about TMDS141.
I'm posting the question for the customer:
++++++++++++++++++++++++++++++++++++++++++++++
We have measured the open circuit voltage of TX2,TX1,TX0,TXC,TX2n,TX1n,TX0n&TXCn pins on TMDS141.
(Vcc=3.3V, OE=High, RXx=Not Connected, TXx pins are not connected with other components. )
The voltage of any TXx pin is about 2.6V.
Why is this voltage generated?
Is it affected by ESD protection or a parasitic diode?
I understand that the "TMDS Output Stage" has no voltage source by seeing the figure
in EQUIVALENT INPUT AND OUTPUT SCHEMATIC DIAGRAMS of the data sheet.
++++++++++++++++++++++++++++++++++++++++++++++
Thank you in advance.
Best regards,
Takishin