Other Parts Discussed in Thread: SN65LVDT386
Hi,
We are planning to connect the LVDS pins of Kintex 7 FPGA to 1A and 1B input pins of SN65LVDS117DGGR.
The implementation is shown in a block diagram attached with the query.
New Microsoft PowerPoint Presentation.pptx
Regarding this connection I have 2 queries :
1. The FPGA LVDS pins reside in 1.8V Bank.The Supply voltage of SN65LVDS117DGGR is 3.3V. I have doubt in IO level compatibilities in this connection.
I was not able to understand the Figure 1 and Table 2 in the datasheet of SN65LVDS117DGGR (see Image 1) and I was unable to compare it against the Output characteristics of Kintex 7 FPGA (see image 2).
Can you confirm whether this connection is possible, whether the output characteristics of FPGA and Input characteristics of SN65LVDS117DGGR are matching?
2. We currently did not provide any termination for LVDS inputs of SN65LVDS117DGGR.In the datasheet, the termination details for all types of IO standard is mentioned except for LVDS. Please inform is any 100 OHM parallel termination or any other type of termination is required for LVDS inputs on 1A and 1B.
Regards,
Nanjunda M