Other Parts Discussed in Thread: DS90CR216A, , DS90CR218A
Team,
My customer want to use FPGA to connect to LCD(RGB666), is below solution ok for customer to use?
They use DS90LV047A and DS90CR216A here as showed above, the signal between FPGA and DS90LV047A is 4 wire LVTTL, the signal between DS90LV047A and DS90CR216A is 4 wire differential, then the serial signal was converted to parallel signal sent to LCD(RGB666).
Why customer don't use differential signal between FPGA and DS90LV047A is because they need 2.5V supply, the number of IO is not enough, so they use LVTTL signal here. So below are support need:
1. If above solution ok for customer to use?
2. If not, why and any other solution for customer to use here?
Best regards,
Sulyn